Advanced Waveform Utility
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:[STATe] ON|OFF|1|0 [:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:[STATe]? |
|
SCPI Example |
|
|
Preset |
OFF |
|
State Saved |
Yes |
|
Range |
ON|OFF |
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:SRATe? |
|
SCPI Example |
|
|
Notes |
This value is the maximal value of contained all segments. |
|
Preset |
50 MHz |
|
State Saved |
Yes |
|
Min |
1e3 |
|
Max |
128e9 |
|
Resolution |
1 |
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:SAMPle:COUNt? |
|
SCPI Example |
|
|
Notes |
When a new waveform file is selected, the sample count will be got and assigned to this setting. |
|
Preset |
10000 Sa |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
1024*1024*1024 |
|
Resolution |
1 |
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:RRATio <real> [:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:RRATio? |
|
SCPI Example |
|
|
Couplings |
When this value is changed, Sample Rate of Waveform will be changed too. If Sample Rate Mode of waveform is manual, then resampling Ratio of carrier can be changed manually. |
|
Preset |
1 |
|
State Saved |
Yes |
|
Min |
0.1 |
|
Max |
Depends on the sample rate and number of samples of imported waveform. |
|
Resolution |
1 |
Set the power boost level of the carrier.
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:POWer <real> [:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:POWer? |
|
SCPI Example |
|
|
Couplings |
Only applied on carrier mixing |
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
-130 |
|
Max |
130 |
Set the frequency offset of carrier.
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:FREQuency:OFFSet <real> [:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:FREQuency:OFFSet? |
|
SCPI Example |
|
|
Couplings |
Only applied on carrier mixing. |
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
-64e9 |
|
Max |
64e9 |
Set the initial phase of carrier.
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:PHASe <real> [:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:PHASe? |
|
SCPI Example |
|
|
Couplings |
Only applied on carrier mixing. |
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
0 |
|
Max |
360 |
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:REPeat:NUMBer <integer> [:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:REPeat:NUMBer? |
|
SCPI Example |
|
|
Couplings |
This setting can be changed only when carrier repeat mode is manual. If carrier repeat mode is auto, repeat number is calculated based on current waveforms. |
|
Preset |
1 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
1000 |
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:TIME:LENGth? |
|
SCPI Example |
|
|
Couplings |
With SCPI, only get action is meaningful. |
|
Preset |
0.001 |
|
State Saved |
Yes |
|
Min |
0 |
|
Max |
1 |
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:FREQuency:COFF <integer> [:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:FREQuency:COFF? |
|
SCPI Example |
|
|
Couplings |
Only used for carrier mixing, when carrier is truncated, appropriated smoothing filter frequency is needed to smooth truncated signal. |
|
Preset |
3000000 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
128e9 |
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:SEGMent:ADD |
|
SCPI Example |
|
|
State Saved |
Yes |
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:SEGMent:DELete <integer> |
|
SCPI Example |
|
|
State Saved |
Yes |
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:Segment:COPY <integer> |
|
SCPI Example |
|
|
State Saved |
Yes |
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:SEGMent:MOVE:UP <integer> |
|
SCPI Example |
|
|
State Saved |
Yes |
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:SEGMent:MOVE:DOWN <integer> |
|
SCPI Example |
|
|
State Saved |
Yes |
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:TIME:OFFSet <real> [:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:TIME:OFFSet? |
|
SCPI Example |
|
|
Notes |
This setting is meaningful only when more than one carrier in waveform. |
|
Preset |
0ms |
|
State Saved |
Yes |
|
Min |
0ms |
|
Max |
10ms |
|
Resolution |
1ps |
Assigns random values to the initial phase of every carrier.
See image.
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:RANDomize:PHASe |
|
SCPI Example |
|
|
State Saved |
Yes |
|
Initial S/W Revision |
A.13.00 |
Resets the initial phase of every carrier to zero value.
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:RESet:PHASe |
|
SCPI Example |
|
|
State Saved |
Yes |
|
Initial S/W Revision |
A.13.00 |